GPIOsetdir & gpiosetvalue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIOsetdir & gpiosetvalue

2,158件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Deepak Bansal on Sat Sep 08 00:08:29 MST 2012
Below are two function in CMSIS code which I use. It works until I have to write single bit, But suppose I have to write 8 bit value on PORT0, then should I have to call this function 8 time. or there is anyway by which I can do this in single call



/**********************************************************************/

void GPIOSetValue( uint32_t portNum, uint32_t bitPosi, uint32_t bitVal )
{
  LPC_GPIO[portNum]->MASKED_ACCESS[(1<<bitPosi)] = (bitVal<<bitPosi);
}

/*****************************************************************************
** Function name:GPIOSetDir
**
** Descriptions:Set the direction in GPIO port
**
** parameters:port num, bit position, direction (1 out, 0 input)
** Returned value:None
**
*****************************************************************************/
void GPIOSetDir( uint32_t portNum, uint32_t bitPosi, uint32_t dir )
{
  if(dir)
LPC_GPIO[portNum]->DIR |= 1<<bitPosi;
  else
LPC_GPIO[portNum]->DIR &= ~(1<<bitPosi);
}
0 件の賞賛
返信
4 返答(返信)

1,814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Deepak Bansal on Sun Sep 09 21:40:10 MST 2012
Hi find a manual but they don't have library description in it.
Or might be I find it wrong.
Can you please refer what manual are you referring.
0 件の賞賛
返信

1,814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Sat Sep 08 10:26:53 MST 2012
LPC_GPIO[portNum]->MASKED_ACCESS[MY_BIT_MASK] = MY_VALUE;

And, why don't you Read The Fine Manual?
0 件の賞賛
返信

1,814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Deepak Bansal on Sat Sep 08 02:12:38 MST 2012

Quote: gbm
You don't need to call any function. Just write the bits you want to the port, optionally using masking so that you update only the selected bits.
And, don't forget to Read The Fine Manual.




Hey I tried the above functions by oring bits. But didn't work for me.
like Bit0 | Bit 1 in fuction call.
0 件の賞賛
返信

1,814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Sat Sep 08 01:14:16 MST 2012
You don't need to call any function. Just write the bits you want to the port, optionally using masking so that you update only the selected bits.
And, don't forget to Read The Fine Manual.
0 件の賞賛
返信