GPIO Remap LPC1788

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Remap LPC1788

724 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by irvind on Mon Jan 07 00:13:39 MST 2013
Hi,

May I ask if we can do a GPIO remap? If yes please provide me the function.

Currently my QEI_PHA,QEI_PHB,QEI_IDX were used by LCD.Is there any method I can remap this QEI interface to other GPIO? I did some remap on STM32 before, so please help me on NXP MCU.

Thanks. :(:(
0 Kudos
Reply
1 Reply

697 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by irvind on Tue Jan 08 21:47:37 MST 2013
According to LPC1788 specification,

LCD need LCD_VD[15:12] for green color, LCD_VD[23:20] for blue color. (minimum requirement)

QEI_PHB pin assigned to P1.23
LCD_VD[13] assigned to P1.23 or P1.27
LCD_VD[21] assigned to P1.27

So if you need to use QEI_PHB function, P1.23 won't be an option for LCD_VD[13], it can only assign to P1.27. Which have conflict with LCD_VD[21] that only can use P1.27.. HOW COME NXP NEVER MENTION no QEI if you need TFT LCD IN DATASHEET!!!!!!!!!!!

Below is their "detail" reply. They even get confused with my part number...
[B][I]Thank you very much for contacting NXP Semiconductor.
It appears that the configuration required by you cannot be achieved on the LPC1768. This is because of the pin multiplexing limitation.[/I][/B]

Anyone got idea how to achieve it? I can achieve it by killing 1 bit of green color, which I think not an ideal solution.
0 Kudos
Reply