Function List

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Function List

1,153 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dirtyBits on Sun Apr 24 04:41:34 MST 2011
Dear All,
I'm new to LPCXpresso and was wondering if there is a [B]list of all the functions[/B] that can be used by LPCXpresso/Code_Red ??

Something like Arduino [B]reference[/B] !?
http://www.arduino.cc/en/Reference/HomePage

Thanks
:)
0 项奖励
回复
2 回复数

1,138 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dirtyBits on Sun Apr 24 07:08:17 MST 2011
[B]@paksoft[/B] Thanks a lot! I'll do try that.

Meanwhile I have LPCXpresso so why don't discover it? I searched the [B]HELP[/B] portion of LPCXpresso IDE and found that there are some [B]predifined Macros[/B] which can be found under [B]GNU C Preprocessor[/B].
Just incase someone like me needs it.

Thanks again,
Regards
0 项奖励
回复

1,138 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paksoft on Sun Apr 24 06:48:47 MST 2011
Hi,
   LPCxpresso is based on GCC. If you want Arduino-like compiler, visit to http://leaflabs.com/devices/maple/  :)

Regards,
pak
0 项奖励
回复