FreeRTOS wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS wizard

1,155 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maxmel on Fri Aug 27 01:38:08 MST 2010
[FONT=Cambria]Hi,[/FONT]

[FONT=Cambria]I have got the LPCXpresso v3.4.6 . [/FONT]

[FONT=Cambria]On the previous version of LPCxpresso, there was a wizard to create a freeRTOS project with two empty tasks and the functions [/FONT][B][COLOR=#7f0055][FONT=Cambria]static[/FONT][/COLOR][/B][B][COLOR=#7f0055][FONT=Cambria]void[/FONT][/COLOR][/B][COLOR=black][FONT=Cambria] [B]setupHardware[/B]([/FONT][/COLOR][B][COLOR=#7f0055][FONT=Cambria]void[/FONT][/COLOR][/B][COLOR=black][FONT=Cambria]);[/FONT][/COLOR][B][COLOR=#7f0055][FONT=Cambria]int[/FONT][/COLOR][/B][COLOR=black][FONT=Cambria] [B]main[/B]([/FONT][/COLOR][B][COLOR=#7f0055][FONT=Cambria]void[/FONT][/COLOR][/B][COLOR=black][FONT=Cambria]) with the creation the tasks.[/FONT][/COLOR]

[COLOR=black][FONT=Cambria]On the 3.4.6 I don’t find the wizard does it disappeared? What is the reason?[/FONT][/COLOR]

[COLOR=black][FONT=Cambria]Thank you for your feedback [/FONT][/COLOR]

[FONT=Calibri]Regards,[/FONT]
0 Kudos
Reply
3 Replies

1,143 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Aug 27 06:58:00 MST 2010
Actually, it has been pointed out to me that the FreeRTOS wizard should not have been part of the LPCXpresso release, which is why it has now been removed from 3.4.6.

However, if you download the latest FreeRTOS installation, there is a demo app "CORTEX_LPC1768_GCC_RedSuite" which also works for LPCXpresso.
0 Kudos
Reply

1,143 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maxmel on Fri Aug 27 06:12:37 MST 2010
Do you know when the release will be available ?
Thankyou
0 Kudos
Reply

1,143 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Aug 27 06:09:02 MST 2010
An updated version will be available in the next release, which uses a more recent release of FreeRTOS
0 Kudos
Reply