Flash programming in LPCXpresso or RedSuite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash programming in LPCXpresso or RedSuite

694件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Mon Jun 13 07:34:52 MST 2011
Hi.
How can I program my target device without using Debug or Run mode in LPCXpresso or RedSuite?
I mean: I have my executable file after compile step: how can I deploy it directly in the device without launching debug session? Is there an external tool to do it?
Thanks a lot
0 件の賞賛
返信
1 返信

680件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jun 13 07:40:28 MST 2011
"Program Flash" button (little chip icon) on the toolbar

or command line:

http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming
0 件の賞賛
返信