Flash memory and Data memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash memory and Data memory

867 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by karthik.s on Wed Aug 04 02:58:17 MST 2010
I am using LPC1114.After building the application the following statistics are displayed on the console window.

text       data        bss        dec        hex    filename
  23892         32       5358      29282       7262    SampleSPI.axf

What i understand is text section indicates the amount of memory occupied in Flash(32KB).

What about the amount of RAM occupied by the application code?

Is it (data+bss)??

Original Attachment has been moved to: 1100583_UART.zip

0 项奖励
回复
1 回复

749 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Aug 04 03:40:50 MST 2010
http://knowledgebase.nxp.com/showthread.php?t=522
0 项奖励
回复