Content originally posted in LPCWare by TheFallGuy on Tue Jan 31 09:58:03 MST 2012
Try this:
- start LPCXpresso
- create a project
- On the Project name in the bottom right corner of the IDE, Press Ctrl at the same time as clicking the mouse. This opens a command prompt, using the same settings as used by the IDE
- in the command prompt, type echo %PATH%
- in the command prompt, type ipconfig
This will show the PATH used by LPCXpresso, and also whether you can see ipconfig. Post the output from the commands