Flash Sector reservation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Sector reservation

612 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Fri Jun 11 04:50:22 MST 2010
I need to use a flash sector for store the application data.
This data will be write and read with IAP command.
Therefor in this sector I don't want code.
How can I configure LPCExpresso linker for not use a particular sector ?
The linker should not put  code in the sector used for data, this sector could be in half to memory!
0 Kudos
Reply
1 Reply

599 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Jun 11 05:29:27 MST 2010
Please see "Using your own linker scripts" at:

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/31

There are multiple previous forums entries on this area as well. I suggest you google for "[I]flash sector site:knowledgebase.nxp.com[/I]" or "[I]iap site:knowledgebase.nxp.com[/I]".

Regards,
CodeRedSupport
http://http://lpcxpresso.code-red-tech.com/LPCXpresso/node/31
0 Kudos
Reply