Flash Programming binaries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programming binaries

990 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoeMoney on Fri Apr 23 17:38:46 MST 2010
When I debug the program, it run fines on the lpc1114 board. But when i tried to directly program the binary using "Program Flash..." from the Binary Utilities, it doesn't run as it suppose to like its waiting for the run command... are there additional steps to the lpc1114 board when using Program Flash to make the program run?

Original Attachment has been moved to: 1100328_blinky_main.zip

0 Kudos
Reply
1 Reply

814 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Apr 24 09:37:03 MST 2010
After programming the flash, the utility leaves the target halted. If you reset or power cycle the device then it will start running the code you have programmed.
0 Kudos
Reply