Flash Programming binaries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programming binaries

952件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoeMoney on Fri Apr 23 17:38:46 MST 2010
When I debug the program, it run fines on the lpc1114 board. But when i tried to directly program the binary using "Program Flash..." from the Binary Utilities, it doesn't run as it suppose to like its waiting for the run command... are there additional steps to the lpc1114 board when using Program Flash to make the program run?

Original Attachment has been moved to: 1100328_blinky_main.zip

0 件の賞賛
返信
1 返信

776件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Apr 24 09:37:03 MST 2010
After programming the flash, the utility leaves the target halted. If you reset or power cycle the device then it will start running the code you have programmed.
0 件の賞賛
返信