Extract data of variable in debug mode in excel or notepad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Extract data of variable in debug mode in excel or notepad

641 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Shoaib on Sun Sep 14 14:25:30 MST 2014
Hi everyone,

I am a newbie to LPC1769 and was doing some experiments using it. I want to analyze the values taken by a variable in the debug mode. Is there any way I can get all the values with respect to time from the start in debug mode.

Thanks,
0 Kudos
Reply
2 Replies

621 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Shoaib on Tue Sep 16 10:25:28 MST 2014
Thanks for the reply!
0 Kudos
Reply

621 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Sep 14 23:51:00 MST 2014
This is supported via LPCXpresso's "SWO trace".  See the "Red Trace" chapters of the LPCXpresso 7 User Guide for more details. Note that currently this will require the use of a 'Red Probe' as you debug probe. Note that as detailed here, only limited stocks of this probe are available.

Regards,
LPCXpresso Support
0 Kudos
Reply