Extra includes entry in LPCxpresso Projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Extra includes entry in LPCxpresso Projects

1,180 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by skamal on Sun Nov 16 12:59:48 MST 2014
I am new to LPCxpresso, which explains why I have this problem. Any time I create a new project, I always see an entry called "I2C_Test/inc" under the includes, along with the CMSISv2p00_LPC17xx/inc that I expect to see. And it is always grayed out. A while back when I started with LPCxpresso, I had created a project called "I2C_Test", so I must have entered its name somewhere which is causing the new projects to put it under the includes. It has been a while since then and I haven't used LPCxpresso since then, so I just can't figure out what I had changed. I have looked at the Preferences and project settings, but haven't found it yet.
I have attached a screenshot of the Project Explorer, showing the I2C_Test/inc. I have exported the I2C_Test into an archive (.zip file) and removed the project from the workspace, which is why I think the exclamation icon is shown.
I would like to reset whatever is causing this extra includes entry. Any help would be appreciated.
0 Kudos
Reply
2 Replies

1,156 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by skamal on Thu Nov 20 13:43:15 MST 2014
Thanks for the reply. The "LPCOpen" in the project name was a misnomer - I intended to link to CMSIS. Anyway, I have downloaded the LPCOpen 2.1 and also updated the LPCXpresso to 7.5 (was using 6.2). Haven't tried it out yet, but I think I understand how to proceed with the LPCOpen and I don't think I will see the original issue anymore now that I have completely removed the old LPCxpresso files.

Thanks for pointing out the new direction.

Best regards.
0 Kudos
Reply

1,156 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 17 03:18:00 MST 2014
Exactly how are you creating new projects : using the "Quickstart -> New project" wizards?

For more details of creating new projects, make sure that you have read the supplied LPCXpresso User Guide, and also watched the "Rapid Embedded Development with LPCXpresso " video at:

http://www.lpcware.com/lpcxpresso

One thing I would note is that you are creating a project called 'UART_LPCOpen", yet you appear to be linking this to an old CMSIS project? As detailed in the USer Guide, we would generally advise sticking to using LPCOpen.

If you are are still having problems, please can you export your project and post. And also confirm the version of LPCXpresso being used.

http://www.lpcware.com/content/faq/lpcxpresso/how-importexport-projects

Regards,
LPCXpresso Support
0 Kudos
Reply