Exemple code for Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Exemple code for Ethernet

1,373 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kevin on Wed Mar 20 06:49:06 MST 2013
anyone have any project using Ethernet as an example to help me
0 Kudos
Reply
4 Replies

1,338 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kevin on Thu Mar 21 07:00:58 MST 2013
Thank you, most do not get to see the example that you send.
This example uses the "stack"?
0 Kudos
Reply

1,338 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Mar 21 06:39:24 MST 2013
There is also the uip example in the same example bundle.

See http://support.code-red-tech.com/CodeRedWiki/RDB1768cmsisExampleProjects
0 Kudos
Reply

1,338 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kevin on Thu Mar 21 06:05:15 MST 2013

Quote: wrighflyer
Your question is a bit vague as you haven't even said which model of LPC but if I guess at LPC17xx then in my copy of CodeRed if I use File-Import then under General using "Existing Projects into Workspace" then [Next>] and select "Select archive file" and use the file selector to open ..\LPCXpresso_5.0.14_1109\lpcxpresso\Examples\NXP\LPC1000\LPC17xx\RDB1768cmsis2.zip then, for example, there seem to be some Ethernet using projects in there. If you look around I'm sure you'll find more.

WF1903



I'm using the LPC1768. I need to make the communication between the computer and the micro-controller, however already tried using the example code "EASYWEB" no longer works.

you have some suggestion.
0 Kudos
Reply

1,338 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wrighflyer on Wed Mar 20 10:54:26 MST 2013
Your question is a bit vague as you haven't even said which model of LPC but if I guess at LPC17xx then in my copy of CodeRed if I use File-Import then under General using "Existing Projects into Workspace" then [Next>] and select "Select archive file" and use the file selector to open ..\LPCXpresso_5.0.14_1109\lpcxpresso\Examples\NXP\LPC1000\LPC17xx\RDB1768cmsis2.zip then, for example, there seem to be some Ethernet using projects in there. If you look around I'm sure you'll find more.

WF1903
0 Kudos
Reply