Examples for LPC812

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Examples for LPC812

1,407件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Mon Jan 14 06:04:03 MST 2013
Just received an Embedded Artist board with LPC812 and also installed LPCXpresso 5.0.14. However, I can not find any examples for this CPU at NXP.

I need to design a program using 2 UARTs and it would be nice to have an example that sets up the right version of CMSIS, CPU type, paths and include files. Should I try to import an LPC1100 example and try to modify it?
0 件の賞賛
返信
2 返答(返信)

1,255件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Mon Jan 14 06:32:41 MST 2013
I didn't know they were included. Looked at the FAQ and http://ics.nxp.com/support/lpcxpresso/- Nothing for LPC 800.

Thanks anyway!
0 件の賞賛
返信

1,255件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Mon Jan 14 06:23:50 MST 2013
And your reason for not importing and using the LPC800 examples supplied in LPCXpresso as a starting point is ?????

C:\nxp\LPCXpresso_5.0.14_1109\lpcxpresso\Examples\NXP\LPC800\NXP_LPC8xx_SampleCodeBundle.zip


HTH!
0 件の賞賛
返信