Example project for AN10955

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example project for AN10955

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Tue Sep 07 22:20:13 MST 2010
Is there any example for use the AN10955 for software uart with a timer?
0 件の賞賛
返信
4 返答(返信)

1,294件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Wed Sep 08 20:24:56 MST 2010

Quote: CodeRedSupport
The application note is available from NXP's website at:
http://ics.nxp.com/support/documents/microcontrollers/?search=an10955&Search.x=0&Search.y=0

Download this zip file and unzip it. Inside you will find a PDF of the document itself, together with the example code - including the project ZIP files suitable for use with the LPCXpresso IDE.

Regards,
CodeRedSupport


Thanks a lot, I will try to configure in 9 bit mode data,1 start bit, 1 stop bit, any advice?
0 件の賞賛
返信

1,294件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Sep 08 06:24:48 MST 2010

Quote: thinkchip
thanks, but where are this zip files? In what version of lpcxpresso is comming?



The application note is available from NXP's website at:
http://ics.nxp.com/support/documents/microcontrollers/?search=an10955&Search.x=0&Search.y=0

Download this zip file and unzip it. Inside you will find a PDF of the document itself, together with the example code - including the project ZIP files suitable for use with the LPCXpresso IDE.

Regards,
CodeRedSupport
0 件の賞賛
返信

1,294件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Wed Sep 08 05:04:56 MST 2010

Quote: CodeRedSupport
Bit confused as to what you are asking for here. From a quick skim of the apps note it appears to use a timer....



And example projects for use with LPCXpresso are provided. You just need to use the "Import" option in the quickstart panel, and navigate to the LPCXpresso_Soft_UART_1343.zip or LPCXPresso_Soft_UART_1114.zip as appropriate.

Regards,
CodeRedSupport



thanks, but where are this zip files? In what version of lpcxpresso is comming?
0 件の賞賛
返信

1,294件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 07 23:32:52 MST 2010
Bit confused as to what you are asking for here. From a quick skim of the apps note it appears to use a timer....


Quote:
This solution relies on a general purpose 32-bit timer and its ability to toggle a dedicated pin while simultaneously monitoring the state of another pin.



And example projects for use with LPCXpresso are provided. You just need to use the "Import" option in the quickstart panel, and navigate to the LPCXpresso_Soft_UART_1343.zip or LPCXPresso_Soft_UART_1114.zip as appropriate.

Regards,
CodeRedSupport
0 件の賞賛
返信