Error while launching command: arm-none-eabi-gdb--version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while launching command: arm-none-eabi-gdb--version

2,205 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jone1316 on Sat Feb 06 20:57:54 MST 2016
I am new to LPCXpresso and just received my LPCXpresso1769 board. I downloaded version 8.0.0. I am able to build a program but can't get it to debug. I have read through much of the forum for and answer that work, but found none.
My path variable is
C:\WINDOWS\system32;
C:\WINDOWS;
C:\WINDOWS\System32\Wbem;
C:\WINDOWS\system32\WindowsPowerShell\v1.0

Please help,
Wes

Original Attachment has been moved to: myTest_error.zip

0 Kudos
Reply
3 Replies

1,929 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 08 01:14:39 MST 2016
Please post the debug log:

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/debug-log
[/list]

Please also spawn a command shell from within the LPCXpresso IDE and see what the path is set to:

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/status-bar-shortcuts
[/list]

From within this command shell, please also enter the following command and post the text output:

arm-none-eabi-gdb --version


Finally, please can you confirm the exact version of Windows that you are running?

Regards,
LPCXpresso Support
0 Kudos
Reply

1,929 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jone1316 on Sun Feb 07 10:56:10 MST 2016
LPCXpresso1769 with CMSIS-DAP probe
Evaluation board OM13085.

The exact same thing.
0 Kudos
Reply

1,929 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Feb 07 03:45:40 MST 2016
We are talking about LPCXpresso1769 rev D?

What's the 'Details' button showing?
0 Kudos
Reply