Error programming with LPCXPresso 3.6.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error programming with LPCXPresso 3.6.1

1,407件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mattoo on Thu Jul 28 12:21:22 MST 2011
Hi All,

When i compile and link my project (MCU = LPC1758) under  LPCXPresso 3.1.2 IDE and then download the hex file with FlashMagic, the download operation is OK.

When i repeat the same operation under LPCXPresso 3.6.1, the download failed. FlashMagic displays the following error message:

ERROR PROGRAMMING THE HEX FILE. ENSURE YOUR RAM BASED FIRMWARE DOES NOT USE RESERVED LOCATION. SEE THE DEVICE MANUAL FOR A FULL DESCRIPTION.

What is wrong with LPCXPresso 3.6.1 IDE ? Does it need some extra settings in RAM configurations compared to LPCXPresso 3.1.2.

Thanks for your helps,

Regards, Mattoo
0 件の賞賛
返信
5 返答(返信)

1,398件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mattoo on Sat Jul 30 04:55:07 MST 2011
in LPCXpresso v4.0.5
0 件の賞賛
返信

1,398件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mattoo on Thu Jul 28 12:52:08 MST 2011
A old one also. I will take the time to evaluate the latest version of LPCXPresso. In the meanwhile, i am curious to know why the hex file produced by LPCXPresso 3.6 can not downloaded whereas it works with version 3.1.2 ?
0 件の賞賛
返信

1,398件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jul 28 12:44:53 MST 2011
Do you want to discuss advantage or disadvantage through updating software with me?

BTW: Which version of FlashMagic are you using?
0 件の賞賛
返信

1,398件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mattoo on Thu Jul 28 12:37:52 MST 2011
If you can not download the hex file under the most recent LPCXPresso IDE, what is the utility to use the up-to-date IDE ?
0 件の賞賛
返信

1,398件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jul 28 12:24:26 MST 2011
Are you aware that the rest of the world is working with V4.0.5 :eek:
0 件の賞賛
返信