Error launching emulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error launching emulator

1,407件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LynnF on Sun Apr 11 13:45:41 MST 2010
Can you tell me what this error is and how to correct?

Error Launching Debug\program name.axf
02: Failed to connect: Ee(02). Not connected to emulator.
0 件の賞賛
返信
4 返答(返信)

1,399件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LynnF on Mon Apr 12 08:37:43 MST 2010
Thanks, I will try some of these.

Thanks for the link; however I did search for information yesterday and that link I did not see.


Later update:
I was able to  ground pin O_1 and recover.
0 件の賞賛
返信

1,399件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 12 07:28:51 MST 2010
In that case, this is likely caused because the last application you were running has tried to set the clock speed to an invalid value. This has been discussed a number of times on the forum. For example, see:
http://knowledgebase.nxp.com/showthread.php?p=1450#post1450
0 件の賞賛
返信

1,399件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LynnF on Mon Apr 12 06:07:40 MST 2010
I am using a LPCXresso with a 1343. I have downloaded to this board many times without issue. Now I get the error. So I tried another board (always have spares) and it works perfectly without error.

However I need to use the first one as it has pins soldered to it for my application.
0 件の賞賛
返信

1,399件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 12 01:19:03 MST 2010
It means it can't find the emulator... i.e. The LPC-Link.

You need to post some details of what you are trying to do, including what you host OS is, and what you are trying to connect to, if we are to be able to help further.

You might also want to read:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/47
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/45
(login required)
0 件の賞賛
返信