Error debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error debugging

2,921件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joe912 on Thu Mar 25 16:55:06 MST 2010
I just received the LPCXPRESSO and have not been able to get the ide working with the board.

Windows xp Sp2
Running under VMware.

i connect the board and the red light on the lpc1114 side begins to blink, and windows prompts me with a driver installation.  i tried directing it to the drivers folder in the lpcxpresso folder, and allowing windows to search for it.   the drivers install and it appears as USB device with DFU capabilities.

  so i start the IDE and load the blinky example. hit build then debug.  the IDE reaches 57% and freezes and gives me a No Emulator or board available error.

i have tried the HID check box from the prefrences window.

i never see any window regarding the installation of the lpc-link drivers.

also as a side note i cant get my software to activate.

thanks for your help
0 件の賞賛
返信
5 返答(返信)

2,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Mar 27 10:05:36 MST 2010
Please contact us at:
http://www.code-red-tech.com/contact.php

and we will help you through this problem.
0 件の賞賛
返信

2,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joe912 on Sat Mar 27 09:48:06 MST 2010
i can get it to work using the script bootLPCXpresso.cmd
then the lpc-link activates and  i am able to debug

so now that im able to debug i would like to be able to activate my product.
however ive tried a few times and it always says invalid activation code
0 件の賞賛
返信

2,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Mar 27 00:44:37 MST 2010
This error means what it says - it can't find the LPC-Link after booting it.

After receiving the error, can you open Device Manager and see if you can find a new device "LPC-Link". If not, look through your USB Devices in VMWare and/or your host computer.
0 件の賞賛
返信

2,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joe912 on Fri Mar 26 14:45:30 MST 2010
i just tried this and it still gives me the same error.

i also tried to reboot into windows and attempt to debug.  Same error.
0 件の賞賛
返信

2,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Mar 26 01:27:26 MST 2010
Hi,

Please read this knowledgebase article to help resolve the issue.

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/47
0 件の賞賛
返信