Error While Lunching Debgue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error While Lunching Debgue

2,150件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Bahadur_Kar on Sat Aug 15 21:22:09 MST 2015
Dear Sir,

I have an LPCXpresso/mbed Base Board rev B from (C) Embedded Artist AB 2010. It was working fine but currently I am having some trouble. Please help on this regards.

The code that I want to run in the board is upload for your reference (File name is "code.jpg").

[img]https://www.lpcware.com/system/files/Code.jpg[/img]

While press "Debug 'Lab1'[Debug]" I am getting some error which also updated for your reference(File names are "Error 1.jpg", "Error 2.jpg").

[img]https://www.lpcware.com/system/files/Error%201.jpg[/img]
[img]https://www.lpcware.com/system/files/Error%202.jpg[/img]

Please Help me on this issue.

Thanking You,

Bahadur Kar
Bangladesh
0 件の賞賛
返信
1 返信

2,111件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Aug 16 07:08:06 MST 2015
What version of LPCXpresso IDE are you using?

What target MCU board do you have plugged into the baseboard?

How are you powering the baseboard? Note in particularly that powering from just the debug USB connector on the target MCU board is not likely to be sufficient.

Have you tried debugging the MCU board when it is not plugged into the baseboard?

Have you tried booting the MCU board into ISP mode?

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
[/list]

Please also double check the jumpers on your baseboard against the Embedded Artists documentation:

[list]
  [*]http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php
[/list]

If you are still having problems, please respond to the above points and also post the debug log generated by LPCXpresso IDE when you start a debug session.

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/debug-log
[/list]

Regards,
LPCXpresso Support
0 件の賞賛
返信