Error 37 while browsing Registers tab

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error 37 while browsing Registers tab

1,379件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert hulsebos on Thu May 12 02:29:40 MST 2016
We are using LPCXpresso v7.9.2 for building various LPC1769 projects. With one project we have hard fault situation that I am investigating. The fault occurs only when the compiler optimization setting is set at -Os (optimize for size), it does not occur when I set it at other levels. (for example -O3)
The problem I have is with the Registers tab of the Develop perspective: When using -O3 optimization, all works well and all registers on the Registers tab are displayed as expected. When I debug the same code, but this time compiled with -Os, then an 'error 37: unknown peripheral name : faults' message is displayed while trying to browse the processor registers. The attachment contains all relevant screen copies... it is an annoying bug, as especially in the situation of a fault one would like to inspect the fault registers...
0 件の賞賛
返信
2 返答(返信)

1,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun May 15 09:35:31 MST 2016
I can't see how the compiler optimisation level could have any affect like this. Can you zip up and post the .log file from the .metadata folder in your workspace?

Also, it would be interesting to know if you see the same issue using the current LPCXpresso IDE v8.1.4?

Regards,
LPCXpresso Support
0 件の賞賛
返信