Error 2 while Installing Link2 Driver with german W8 PRO / 32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error 2 while Installing Link2 Driver with german W8 PRO / 32

937件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Jun 17 03:53:52 MST 2013
Just tried to update a german W8 PRO /32 PC to  LPCXpresso v5.2.4 [Build 2122] [2013-04-29].

Got a message:

[ATTACH]1059[/ATTACH]

and the driver isn't installed:

[ATTACH]1060[/ATTACH]

Trying to install it online or local failed:

[ATTACH]1061[/ATTACH]

Is there a known issue with german W8/32? Is there someone out there who is using this version and Link2?

Note: LPCXpresso is working without problems and LPC-Link. Anti-Virus & Firewall are off.
0 件の賞賛
返信
3 返答(返信)

930件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jun 19 00:45:33 MST 2013
I have just double-checked, and it all works perfectly on our Win8/32 bit machine.

In my experience, this error is normally associated with a bad install of Win8 - possibly the driver database has become corrupted?
0 件の賞賛
返信

930件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Jun 18 01:37:26 MST 2013
It's customer PC, which I use with remote support software (TeamViewer) to program / test things. Not sure why it's 32 bit. Probably because it's an 30€ WIN8 Update from Vista PRO 32.
I've noticed that Link2 has less problems with power saving (at least with W7). With Link there are problems to recognize it after 'Sleep Mode' (reconnecting USB is solving that), therefore Link2 looks like the better choice.
0 件の賞賛
返信

930件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jun 17 23:58:31 MST 2013
No known issues here - we'll look into it.

Out of interest though, why Win8/32 rather than 64bit? Is this by choice or due to hardware limitations on your PC?

Regards,
CodeRedSupport
0 件の賞賛
返信