Egit and LpcXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Egit and LpcXpresso

799 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Mon May 23 10:26:41 MST 2011
I found that installing Egit in LpcXpresso as others IDEs based on Eclipse (this is a problem also fo Eclipse CDT Helios) doesn't work properly. More exactly creating a repository or accessing Window/Preferences/Team/Git/Configuration hangs up LpcXpresso/Eclipse. In other forums there are some suggestions to solve the problem that seems to be related only to Windows installations; some indicates the origin to the presence of cygwin on the path, some other reasons. From these solutins one that works for me is to append at the end og lpcxpresso.ini this line:
-Djgit.gitprefix=C:/ProgrammiX86/Git/etc

in my installation this is the root of git installation so you have to change with the correct one for yours. If you have any doubt you may search for gitconfig (that is present on your git root folder). This procedure for me work also for Eclipse (you have to modify eclipse.ini) and for Red Suite 3 (redsuite3nxp.ini).
0 Kudos
Reply
1 Reply

764 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert.palmer on Wed Mar 28 13:38:05 MST 2012
I had trouble just installing Egit.  It said it needed mylyn, which wasn't installed by default, then when I tried to install mylyn, it said it needed something else which I couldn't find.

Did you have similar issues installing Egit or do you have suggestions on resolving the issue?
0 Kudos
Reply