Easy Config LPC175x/6x Microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Easy Config LPC175x/6x Microcontroller

1,229件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Noboru on Mon Mar 17 16:44:57 MST 2014
Hi friends,

I'm providing software to help develop programs to LPC175x/6x microcontrollers with LPCXpresso IDE.

If someone interest to test and report the errors, will be welcome.

The software is free.

Best regards,
Alberto.

Original Attachment has been moved to: Easy%20Config-setup.rar

0 件の賞賛
返信
2 返答(返信)

1,173件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Noboru on Tue Mar 18 13:00:48 MST 2014
Hi TheFallGuy,

The file is .RAR because the forum doesn't accept executable file. Yes, is executable file. Why I share?

Because I want to offer a free tool to help the community that program LPC175x/6x microcontroller in Brazil and other countries.

The file can be download in my site too. www.albertonoboru.com.br

When I finish the first video tutorial about the program in You Tube, I will post the link.

In my site, there is some information about the BROH project too. It is a open hardware project that it will be avaliable to download on April.

Best Regards,
Alberto Noboru Miyadaira
0 件の賞賛
返信

1,173件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Mar 18 01:34:47 MST 2014
I see you have posted a Windows executable file within the .RAR file. I would strongly recommend that you DO NOT run this executable as we there is no way to verify its contents (without running it).

Please explain exactly what it is you are posting and why.
0 件の賞賛
返信