EM773 development

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EM773 development

802 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Kamyar on Wed Dec 04 10:52:16 MST 2013
Hi there,

I am newbie in using LPCware platform for software development of EM773 energy metering chip. First of all, is EM773 still supported by NXP as I could not find free softwares for this chip in their website. If it is not supported, where can I find EM773 software examples and application notes?

I intend to use EM773 for our energy optimization solution. I need to communicate with the chip through the USB serial line for development, and also wireless communication for the users' display (PC or mobile). I know that all of these is provided with EM773 development kit. However, since I want to use EM773 MCU to prototype our product, I need the schematics and connections for connecting the MCU unit for USB and wireless communications. Where can I access to such schematic?

I have a good experience in developing embedded software for mbed LXP1768. Developing for mbed is very easy via the cloud service that ARM provided. Is programming EM773 only possible with LPCware platform? If it is, where can I find the debugger and start programming the chip? Do I need any other tool?

Regards,

Kamyar
0 Kudos
Reply
1 Reply

778 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Dec 04 11:04:14 MST 2013
Googling EM773 produces the product page on the main NXP website. Seem to be docs and an SDK available…

http://www.nxp.com/products/microcontrollers/application_specific/EM773FHN33.html#documentation

HTH!
0 Kudos
Reply