Download HEX from Target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Download HEX from Target

1,560件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ajacks504 on Thu Feb 20 10:45:37 MST 2014
Hi guys,

I'm looking for an easy way to download the binary from one target, then put it on another.

Any ideas?

Thanks,
Adam
0 件の賞賛
返信
5 返答(返信)

1,520件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ajacks504 on Thu Feb 20 13:17:25 MST 2014
Thanks for your response.

I was originally thrown off by this comment on the link support provided:


Quote:
In the same way, you can use the "Import" icon to allow a memory to be written to. Note that this does not allow Flash memory to be programmed.



I'll give it a shot.
0 件の賞賛
返信

1,520件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Thu Feb 20 13:09:36 MST 2014

Quote: ajacks504
Any ideas?



FlashMagic supports all ISP modes (which is usual Serial and CAN).

If you want to use Ethernet, you have to use a secondary bootloader.

LPCXpresso can export all memory regions (Flash, RAM....) in different file formats.

Just start a debug session. Use 'Attach only' (Launch configuration->Debugger) to connect an unknown flash...
0 件の賞賛
返信

1,520件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ajacks504 on Thu Feb 20 12:43:17 MST 2014
Well, I'm still not there actually.

I want to download the FLASH contents from a LPC1114/302 using my LPC1114 LPC-Link eval board.

The link above only lets me get the RAM contents it looks like, and it seems Flash Magic only supports serial or ethernet interfaces?\

Any ideas?
0 件の賞賛
返信

1,520件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ajacks504 on Thu Feb 20 12:26:52 MST 2014
Thanks for that, I ended up using Flash Magic:

http://www.flashmagictool.com/
0 件の賞賛
返信

1,520件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 20 12:15:29 MST 2014
See: http://www.lpcware.com/content/faq/lpcxpresso/import-export-memory

Regards,
LPCXpresso Support
0 件の賞賛
返信