Difference between debug and trace functionality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between debug and trace functionality

2,090件の閲覧回数
prachipanse
Contributor III

Hi,

Where can I find the difference between the debug and trace functionalities? What features are present in each?

Regards,

Prachi

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,900件の閲覧回数
thefallguy
Contributor IV

Debug and trace are two different, but complementary things. Very briefly:

  • Debug allows you to interact with the processor to examine its state while it is executing your application. You can stop, examine registers, peripherals and memory, step through code to examine its effects etc.
  • Trace records certain aspects of what your processor *has done*. That is, the application is running at full speed and trace can be switch on/off to record (for example) what instruction have been executed, and/or what data has been read/written to memory Cortex-M3/M4 have some trace capabilities built into the processor and allow you to trace accesses to a few memory locations and (if the *optional* ETM/ETB is implemented in the processor) the instructions executed. Cortex-M0+ allows some limited instruction tracing via the MTB.

*EDIT*: Note that not all NXP Cortex-M3/M4 parts have the instruction trace capability as the ETM/ETB has not been implemented in the processor. So, LPC17, LPC15 and LPC13 do not have instruction trace, but the LPC18, LPC43 do.

You can find more information here

http://www.nxp.com/assets/documents/data/en/user-guides/LPCXpresso_IDE_Instruction_Trace.pdf 

0 件の賞賛
返信

1,900件の閲覧回数
prachipanse
Contributor III

Hi,

This clarifies. Thank you.

Regards,

Prachi

0 件の賞賛
返信