Defining Pin Function in Software

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Defining Pin Function in Software

1,036 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pleonhardt on Sun May 18 11:34:44 MST 2014
I have the LPCXpresso software up and running and am able to run example programs with demo boards.  I am now to the point where I would like to design my own hardware and modify the function of the software.  Can someone tell me where in the firmware libraries the GPIO pin function is set, for example input/output, etc.?  There must be a large table somewhere, but I am not able to find it.

Thanks.
0 项奖励
回复
2 回复数

1,028 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun May 18 12:19:58 MST 2014

Quote: pleonhardt
I am now to the point where I would like to design my own hardware and modify the function of the software.



Usually UM is including a detailed function description in chapter IOCON  :)
0 项奖励
回复

1,028 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sun May 18 11:42:18 MST 2014
Have an intensive look at http://www.lpcware.com/content/nxpfile/lpcopen-platform.
0 项奖励
回复