Debugmon_handler error?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugmon_handler error?

1,665 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by james on Fri May 03 02:08:19 MST 2013
Hi,

I am using the UEZ1788 touchscreen kit. I have 2 sets which I encountered Debugmon_handler error, aka debug monitor error.

I did a google search and cant seem to find what is the cause of this error? I know the firmware works because I have a few units which works fine loaded with the same firmware.

What should I be looking at?
0 Kudos
Reply
1 Reply

1,128 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Fri May 03 13:18:07 MST 2013
Is this with or without a debugger connected? If you are connected with the debugger then which tools and probe are you using?

I would suspect the most likely cause of this would be to have an BKPT instruction explicitly coded into your actual application code, with no debug tools connected.
0 Kudos
Reply