Debugging without target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging without target

1,525件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Mon Jun 29 03:12:04 MST 2015
Is it possible to debug a project in simulator mode i.e without connecting to the target through debug probe?
0 件の賞賛
返信
6 返答(返信)

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Tue Jun 30 02:10:20 MST 2015
Will check this out. Thank You.
0 件の賞賛
返信

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Jun 29 07:31:01 MST 2015
Try reading the FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/generating-srec-binary-and-ihex-files
0 件の賞賛
返信

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Mon Jun 29 06:17:07 MST 2015
What is the procedure to create a binary file which can be burnt to the FLASH which is present on custom board with LPC3250 processor?
0 件の賞賛
返信

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 29 04:42:15 MST 2015
No. LPCXpresso is a development tool for NXP Microcontrollers. It is not a tool for developing Host applications.
0 件の賞賛
返信

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Mon Jun 29 04:07:37 MST 2015
If we want to run a simple C code which does not require any target, is there any option for that?
0 件の賞賛
返信

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 29 03:45:51 MST 2015
We do not provide a simulator with LPCXpresso. There is a very wide range of developments boards and debug probes available, priced from just a few dollars.
0 件の賞賛
返信