Debugger Pinout for LPC1113

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger Pinout for LPC1113

1,180件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Mon Jun 18 20:41:28 MST 2012
Greetings,

Just got my first board with a LPC1113 working with LPC Link, took me a day to find out that the 3.3V regulator was dead, and there I was looking at the signals from the debugger!

Anyway, I need some advice on the proper connection of the debug signals to the 10 way header on the LPC Link. This is what I have:

1: 3.3V via 0R link.
2: SWDIO
3, 5, 9: 0V
4: SWCLK
6, 7, 8 No Connection
10: /RESET

I have a 10K pullup resistor on /RESET, but no pullups on SWDIO or SWCLK. I was intending to disable debug in released code by setting CRP level 1 & setting these pins to output, so removing the issue of noise pickup on the debug pins.

Do I have this right?
0 件の賞賛
返信
3 返答(返信)

1,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 19 01:59:04 MST 2012

Quote:
Do I have this right?        

Searching in Code Red Wiki shows:

http://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections

Forum search shows:

http://knowledgebase.nxp.com/showthread.php?t=635
0 件の賞賛
返信

1,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Mon Jun 18 23:09:04 MST 2012

Quote: OXO
You only need SWDIO, SWCLK, RESET and GND for a functioning SWD debug on the LPC1113



Actually I have never seen the LPC-Link assert RESET, maybe it only does so if there is no response to data on SWDIO/SWDCLK. I should check this.

Certainly there is no need for any connection to pin 1 for the LPC Link, as it only has a "not fitted" resistor on this pin. Maybe it is required for the bigger debuggers.
0 件の賞賛
返信

1,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Mon Jun 18 22:56:23 MST 2012
You only need SWDIO, SWCLK, RESET and GND for a functioning SWD debug on the LPC1113
0 件の賞賛
返信