Debug hangs with Red Probe +

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug hangs with Red Probe +

614件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Tue Jul 23 02:31:47 MST 2013
I have a project which has previously worked, but now when I come back to it, I can't get the debugger to run.

I'm using LPCXpresso 5.2.4 build 2122 with Red Probe+. Target is our own hardware, LPC11E14.


What happens is the the project compiles fine, but the progress bar gets stuck at 97% Configuring GDB

LPCXpresso Debug Driver v5.2 (Apr 26 2013 19:52:22 - crt_emu_lpc11_13_nxp build 1153)
Looked for chip XML file in C:/nxp/LPCXpresso_5.2.4_2122/lpcxpresso/bin/LPC11E14/401.xml
Looked for vendor directory XML file in C:/nxp/LPCXpresso_5.2.4_2122/lpcxpresso/bin/nxp_directory.xml
Found generic directory XML file in C:/nxp/LPCXpresso_5.2.4_2122/lpcxpresso/bin/crt_directory.xml
Emu(2): Conn&Reset. DpID:  BB11477. Info: FTVBCVDDA
SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Packet delay: 0  Poll delay: 0.
Loaded LPC11_12_13_32K_8K.cfx: LPC11_12_13 (32K Flash, min 8K RAM) Apr 22 2013 12:14:02  On-chip Flash Memory
NXP: LPC11E14/401  Part ID: 0x00000000
Connected: was_reset=false. was_stopped=false
v Registered license, download limit of 128K


If I ask the IDE to program the AXF file into flash, that works fine, so the debugger hardware is working.
0 件の賞賛
返信
1 返信

591件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 23 12:16:21 MST 2013
Can you try booting into ISP, then try connecting?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip

If the GUI flash programmer is working, can you try mass erasing before debugging - does your debug session then work?

http://support.code-red-tech.com/CodeRedWiki/GuiFlashProgramming

It would also be worth checking power, plus your debug/reset circuitry:

http://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections

Regards,
LPCXpresso Support
0 件の賞賛
返信