Debug failed with j-link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug failed with j-link

907 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarkG on Fri Jun 26 15:58:03 MST 2015
Hi.

I am having a problem debugging LPCXpresso. I am using a segger j-link debugger and configured to the following:

https://www.segger.com/nxp-lpcxpresso.html

When I hit debug (and launch config shown in image 1) I get the following error.

Error in final launch sequence
[img]C:\Users\Mark\Desktop\Image 1.jpg[/img]
-target-select remote localhost:2331

Error message from debugger back end:
localhost:2331: The system tried to join a drive to a directory on a joined drive.
localhost:2331: The system tried to join a drive to a directory on a joined drive.

This is also what appears in the console.

GNU gdb (GNU Tools for ARM Embedded Processors) 7.8.0.20150304-cvs
Copyright (C) 2014 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.  Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.
For help, type "help".
Type "apropos word" to search for commands related to "word".

The hardware is fine as iv used it in different applications.

Any ideas what is causing this?

Thanks,

Mark.
0 Kudos
Reply
0 Replies