Debug command (push run)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug command (push run)

548 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Mon Sep 10 19:02:17 MST 2012
[COLOR=#333333][FONT=Arial]I have a question about the[/FONT][/COLOR][COLOR=#333333][FONT=Arial] LPCXpresso.
Of the following symptoms occur, I will not attempt to smooth the debug.[/FONT][/COLOR]
[FONT=Arial] [/FONT]
[COLOR=#333333][FONT= ]■[/FONT][/COLOR][COLOR=#333333][FONT=Arial]Operation details[/FONT][/COLOR]
[FONT=Arial][COLOR=#333333]If you use the[/COLOR][COLOR=#333333] LPCXpresso IDE, there are times when you do not work correctly [/COLOR][/FONT]
[FONT=Arial][COLOR=#333333]when you run the[/COLOR][COLOR=#333333] Debug command (icon of an insect).[/COLOR][/FONT]
[FONT=Arial] [/FONT]
[FONT= ] [/FONT][COLOR=#333333][FONT=Arial]Stops[/FONT][/COLOR][COLOR=#333333][FONT=Arial] running when you press the Run button.
Stop the execution of that button is not available for the debugger that hardens.[/FONT][/COLOR]
[FONT=Arial] [/FONT]
[FONT= ] [/FONT][FONT=Arial][COLOR=#333333]And[/COLOR][COLOR=#333333] may not occur if the above operation can occur.[/COLOR][/FONT]
[FONT=Arial] [/FONT]
[FONT= ]■[/FONT][FONT=Arial]Q[COLOR=#333333]uestion[/COLOR][/FONT]
[FONT= ] ・[/FONT][FONT=Arial][COLOR=#333333]Is there any way to[/COLOR][COLOR=#333333] the above operation can be improved?[/COLOR][/FONT]
[FONT= ]・[/FONT][FONT=Arial]Has it checked in your company about the above-mentioned operation?[/FONT]
0 项奖励
回复
0 回复数