Debug button off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug button off

904 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Thu May 12 00:11:24 MST 2016
LPCXpresso v8.1.4 [Build 606] [2016-03-14]
LPC1758
LPCLink

Yesterday everything worked well, this morning however after connecting with LPCLink the play buttons, steps are not active !!
The LPCLink connects properly, the green line is in the mai first line, but the debug button is off !!

What may have happened ?

Thanks
0 Kudos
Reply
2 Replies

813 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

813 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Fri May 13 02:33:06 MST 2016
After many test . . . solved the problem changing the prospecrive from debug to develop and then restart the lpcxpresso application.
0 Kudos
Reply