Debug Issue: @ startup or IDE reset end up in endless loop at x1fff00d6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Issue: @ startup or IDE reset end up in endless loop at x1fff00d6

1,145 次查看
jimprince
Contributor I

Debug Issue: No startup or IDE reset end up in endless loop at x1fff00d6.

Using LPC824Max board.

Environment:

Version: LPCXpresso v8.1.4 [Build 606] [2016-03-14]

Operating system: Windows 8.1

VM: Java HotSpot(TM) Client VM (32 bit)

 

This is a "Pro" license: How do I get the promised support that I paid for?

 

What is at x1fff00d6 ?

How do I fix this ?

 

This is a tool issue that is wasting days.

 

Thanks. Jim

0 项奖励
回复
1 回复

989 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

The LPC824 is looping in the bootloader. This means it found no flash image it could boot. Either flash is blank, or, the bootloader couldn't validate the checksum word.

Thanks and regards,

LPCXpresso Support

0 项奖励
回复