Dead links

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dead links

810件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xander.houtman on Sat Apr 25 07:33:20 MST 2015
Hello LCP community,

I found a dead link in LPCXpresso.
When pushing the "Help on this error..." button when an error is reported you are directed to a google link which searches the following site:
"http://www.lpcware.com/content/faq/lpcxpresso"

But this site doesnt exist anymore.
0 件の賞賛
返信
1 返信

801件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Apr 25 10:51:51 MST 2015
That address is the root for all of the LPCXpresso FAQs, which you can view the full list of via:

http://www.lpcware.com/faq/lpcxpresso

If you are having problems with the IDE searching the FAQs for a particular error, please detail the actual error being searched for, as well as the google search actually being run.

Regards,
LPCXpresso Support
0 件の賞賛
返信