Data TCP/IP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data TCP/IP

1,544件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRomain on Tue Oct 09 01:48:36 MST 2012
Hello,
I need help for modification soft uIP or EasyWeb. I would like to create a comunication between my computer(Delphi) and the microcontroller without generating the web page.
thank you.
0 件の賞賛
返信
5 返答(返信)

1,523件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Wed Oct 10 03:01:31 MST 2012

Quote: PRomain
Yes I did try to open a TCP connection with it's functions EasyWeb and uIP but the comunication generate a web page. I need create a connection with a soft uIP without generating the web page.



:confused:

EasyWeb is using TCP to establish HTTP :)

So it's including TCP engine. Of course you have to delete HTTP parts ;)
0 件の賞賛
返信

1,523件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRomain on Wed Oct 10 02:45:41 MST 2012
Yes I did try to open a TCP connection with it's functions EasyWeb and uIP but the comunication generate a web page. I need create a connection with a soft uIP without generating the web page.
0 件の賞賛
返信

1,523件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Wed Oct 10 00:40:07 MST 2012
Isn't EasyWeb including TCP?

Did you already try to open a TCP connection with it's functions?
0 件の賞賛
返信

1,523件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRomain on Wed Oct 10 00:18:44 MST 2012
We are talking about TCP
0 件の賞賛
返信

1,523件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ex-kayoda on Tue Oct 09 05:30:50 MST 2012

Quote: PRomain
... a comunication between my computer(Delphi) and the microcontroller...



So we are talking about TCP or UDP :confused:
0 件の賞賛
返信