DFUSec / LPC-Link 2 from Win7 in VirtualBox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DFUSec / LPC-Link 2 from Win7 in VirtualBox

880 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hermaness on Tue Feb 04 09:24:41 MST 2014
Hi,

I'm trying to reflash my LPC-Link 2 with the CMSIS-DAP firmware using a Win7 image hosted in VirtualBox. I registered the "NXP LPC" USB device with the Win7 instance and see the "LPC" listed in "Devices and Printers" in the section "Unspecified".

The DFUSec utility also recognizes the LPC-Link - the "program..." button is enabled and the left image selection header is green. I selected the "CMSIS-DAP LPC-Link 2 debugger image".

Programming fails with sections two and three both red and this status text output:

Programming algorithm cmdResponse: 0
Programming algorithm progStatus: 4

(see screenshot attached below)

Anybody here using a similar setup that could help?
Thanks in advance,

Thomas



0 Kudos
Reply
0 Replies