Cycle Count

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cycle Count

713 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by joumaxi on Fri Jun 17 04:30:13 MST 2011
Hi guys!

Has anyone made counting cycles/timing in debug mode?
Can I perform this task in LPCXpresso using the LPC-Link connected to the embedded application to monitor a main program loop for example?:confused:

Bye,

Joumaxi
0 Kudos
Reply
1 Reply

678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Jun 17 04:44:51 MST 2011
If you are working with M3, you can just use Cycle & Cycle Delta in Core Registers View :)

See:

http://knowledgebase.nxp.com/showthread.php?t=395
0 Kudos
Reply