Cross compiling FLTK with Fluid for Cortex M3 architecture using Visual Studio 2013, any help?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cross compiling FLTK with Fluid for Cortex M3 architecture using Visual Studio 2013, any help?

1,428 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Feb 27 04:11:55 MST 2014
Hi Friends,
I have this customized LPC1788 board, I did manage to port Linux and used FLTK with Fluid to create a GUI. I am not a Linux guy, wanted to do the same thing using Windows. I mean to say I am planning to use FLTK and Fluid in Windows environment.

After going through few tutorials I manage to compile FLTK project in Visual Studio 2013. But I am not getting how to cross compile the same project for Cortex M3 ARM architecture.

Please guide me, it would be a great help if you can guide me to any related tutorial. I have been googling from last two days without much success.

I hope i am not breaking any rules by posting the same post in microcontroller section and here as well. If that so, i request admin to delete  this one.

Thank you!
Average:
0 Kudos
Reply
2 Replies

1,330 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Feb 27 21:45:13 MST 2014
Thanks djlegge,
Yes i have tried emwin, you have very little to for the development with emwin. The source is locked, what we can do with emwin is only a window manager with limited options.

Anyway thanks for your advise, i will try "Buildroot".

Thank you.
0 Kudos
Reply

1,330 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by djlegge on Thu Feb 27 05:01:31 MST 2014
FLTK applications require an X-server (display server) as well as linux to run. You will need something like X11 (tiny-X) or possibly nano-X in addition to linux running on your LPC1788. These display servers use the linux framebuffer device but provide a higher level interface to it (including font drawing etc.). I have used 'buildroot' to build all FLTK, tinyX and nano-X for other ARM devices so maybe that is a place to start ?
As far as I know, buildroot requires a linux PC. Really, any kind of linux development is best done on a linux machine anyway so you will probably need at least a linux virtual machine running for any of these options.
I think there was a port of FLTK to directfb which may worth investigating too but I have no idea how practical these options really are for an LPC1788. They will all need some MB of ram on your board.
Have you tried emwin ? This seems to be what NXP recommend for graphics although I have not used it myself.
Good luck.
0 Kudos
Reply