Could someone share the LPCXpresso training materials from https://community.nxp.com/thread/429508

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Could someone share the LPCXpresso training materials from https://community.nxp.com/thread/429508

跳至解决方案
1,933 次查看
hmyoong
Contributor III

The pptx file  https://community.nxp.com/docs/DOC-330499 from Where can I get training resources for LPCXpresso IDE?  could not be assessed. Could someone post it? As I do not have link with poster, I could not contact him.

1 解答
1,593 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

All the presentations from the NXP FTF 2016 conference are available at : NXP FTF 2016 - Training Presentations 

The LPCXpresso IDE one is at https://community.nxp.com/docs/DOC-331545 

This is a PDF only. You may also want to watch the videos linked to from the LPCXpresso IDE product page at : http://www.nxp.com/lpcxpresso

Regards,

LPCXpresso Support

在原帖中查看解决方案

2 回复数
1,593 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Thanks for spotting the error in the FAQ (it was pointing to the powerpoint source instead of the PDF) ... it should be fixed now.

Regards,

Brendon

0 项奖励
回复
1,594 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

All the presentations from the NXP FTF 2016 conference are available at : NXP FTF 2016 - Training Presentations 

The LPCXpresso IDE one is at https://community.nxp.com/docs/DOC-331545 

This is a PDF only. You may also want to watch the videos linked to from the LPCXpresso IDE product page at : http://www.nxp.com/lpcxpresso

Regards,

LPCXpresso Support