Could someone share the LPCXpresso training materials from https://community.nxp.com/thread/429508

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could someone share the LPCXpresso training materials from https://community.nxp.com/thread/429508

ソリューションへジャンプ
1,920件の閲覧回数
hmyoong
Contributor III

The pptx file  https://community.nxp.com/docs/DOC-330499 from Where can I get training resources for LPCXpresso IDE?  could not be assessed. Could someone post it? As I do not have link with poster, I could not contact him.

1 解決策
1,580件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

All the presentations from the NXP FTF 2016 conference are available at : NXP FTF 2016 - Training Presentations 

The LPCXpresso IDE one is at https://community.nxp.com/docs/DOC-331545 

This is a PDF only. You may also want to watch the videos linked to from the LPCXpresso IDE product page at : http://www.nxp.com/lpcxpresso

Regards,

LPCXpresso Support

元の投稿で解決策を見る

2 返答(返信)
1,580件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Thanks for spotting the error in the FAQ (it was pointing to the powerpoint source instead of the PDF) ... it should be fixed now.

Regards,

Brendon

0 件の賞賛
返信
1,581件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

All the presentations from the NXP FTF 2016 conference are available at : NXP FTF 2016 - Training Presentations 

The LPCXpresso IDE one is at https://community.nxp.com/docs/DOC-331545 

This is a PDF only. You may also want to watch the videos linked to from the LPCXpresso IDE product page at : http://www.nxp.com/lpcxpresso

Regards,

LPCXpresso Support