Corrupt project properties for MCU setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Corrupt project properties for MCU setting

710件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pat on Wed Nov 02 08:25:56 MST 2011
Hi,

Somehow I messed up the MCU setting in the project properties. When I now select 'MCU settings' under 'C/C++ Build' I get a 'Could not accept changes/The current displayed page contains invalid values'. And next a java null pointer exception. But no error output.
The IDE status bar still shows the correct MCU type.

I did a diff of the .cproject file with older revisions and can not find the issue.

Is there a way how to see which 'value' is incorrect in the project settings to fix this?
[Yes I am a bit lazy to recreate the whole projects from scratch]

regards,

Pat
0 件の賞賛
返信
1 返信

669件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pat on Thu Nov 03 00:58:48 MST 2011
Ok, seems to be fixed. Created a new workspace and imported the projects again solved the issue.
0 件の賞賛
返信