Conflict between the debug link and wireless mouse driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Conflict between the debug link and wireless mouse driver

903件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by croopnarine on Fri Dec 02 02:24:54 MST 2011
I'm using the LPCXpresso development board with an LPC1769 MCU 4 and the LPCXpresso  4.1.0 Build 190, on Windows7 OS.

Every time I program, (or just connect to), the MCU via the USB debug Link, the system mouse (wireless, logitec) stops working;  rebooting gets the system back to normal operation.

Is there some conflict between the dirvers?
0 件の賞賛
返信
2 返答(返信)

897件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Fri Dec 02 22:45:21 MST 2011
Is this only when using LPC-Link?
I have a similar problem where my USB microscope camera  stops working whenever I plu in any USB device (even a memory stick).

Rob
0 件の賞賛
返信

897件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Fri Dec 02 18:03:11 MST 2011
It sounds like you may have shorted the USB power to ground.
The system notices the overload and shuts the USB subsystem down.
Generally a reboot fixes it.

Pete.
0 件の賞賛
返信