Configuration IDE in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration IDE in Linux

1,433 Views
rodrigolamoglia
Contributor I

How do I configure the LPCexpress 6.4.1 Linux program?

Linux recognizes the board, but is not recognized in the program, is there any tutorial that I have setup?

0 Kudos
Reply
1 Reply

1,344 Views
lpcxpresso_supp
NXP Employee
NXP Employee

First of all, I would recommend that you update to a more recent version of LPCXpresso IDE (v8.2.2 was the last version) or preferably MCUXpresso IDE (http://www.nxp.com/mcuxpresso/ide) which has superseded LPCXpresso IDE.

Then read the Installation Guide which details various things to note when installing on Linux. For LPCXpresso IDE you can visit the Documentation tab of https://www.nxp.com/lpcxpresso/ , and for MCUXpresso IDE visit MCUXpresso IDE|NXP 

In particular, note the flavours of Linux that we actually support.

If you need more assistance, please clarify what version of Linux you are using, which eval board, and what you do and what messages you actually see in the IDE.

Regards,

LPCXpresso Support

0 Kudos
Reply