Compiler/Linker warnings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler/Linker warnings

652件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bhallett on Fri Oct 01 04:42:19 MST 2010
Hello All,

I have recently removed and re-installed LPCXpresso 3.3.4 (kept version for project compatibility) however ever since having done this I seem to always received the following warning:


Invalid project path: Include path not found (C:\!_ide\nxp\lpcxpresso_3.3.4_170\tools\arm-none-eabi\include).CMSISv1p30_LPC13xxpathentryPath Entry Problem


This does not seem to be causing any problems in the actual project itself but I would like to resolve the issue.

I cannot see anywhere where I can correct this problem, can anyone help ?

Regards

Barry
0 件の賞賛
返信
1 返信

645件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Oct 01 05:55:35 MST 2010
Please see:

http://support.code-red-tech.com/CodeRedWiki/InvalidProjPath

Regards,
CodeRedSupport
[B]
[/B]
0 件の賞賛
返信