Compiler Limit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler Limit

1,337件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Wed Mar 30 02:21:16 MST 2011
Are you all using the full $999 compiler, or is the 128k download limit version enough?

I'm going to do a simple datalogger with USB and CAN. Hoping not to layout the $999
0 件の賞賛
返信
3 返答(返信)

1,331件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 30 02:54:56 MST 2011

Quote:

...simple datalogger with USB and CAN...



= 25-30k :)

If you need more than 128k for a simple CAN -> USB datalogger, you should spend the money for a C training course.

USB: see RDB1768cmsis_usbstack sample (in RDB1768cmsis.zip)
0 件の賞賛
返信

1,331件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Wed Mar 30 02:43:06 MST 2011
128k seems like quite a lot of code space to me. How much space would be used by a USB stack?
0 件の賞賛
返信

1,331件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Mar 30 02:34:01 MST 2011
We offer the LPCXpresso version of our IDE at $0,  and then several Red Suite variants at $256, $512 and $999. Code download limits is just one of the differences between the various products. For more details, including comparisons of what you get in each version, please take a look:

http://support.code-red-tech.com/CodeRedWiki/ProductOverview

Regards,
CodeRedSupport
0 件の賞賛
返信