Command failed with exit code 139 // after wrong uart cfg

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Command failed with exit code 139 // after wrong uart cfg

1,210 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FlySnake on Sun Sep 18 01:00:46 MST 2011
Hello!
I have a problem with programming/debugging LPC1768.
Probably because the CPU goes into hard fault right after startup. It worked OK before I had added uart functionality with wrong settings, and now I cannot do anything with this chip. LPC-link freezes at "15% [Connect] nSRST assert (if available" for a while and then gives me "Command failed with exit code 139". Also I have J-Link adapter, but it doesn't work too.
Please, help me bring the chip back to live
0 项奖励
回复
2 回复数

1,185 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FlySnake on Mon Sep 19 01:42:24 MST 2011
Thanks for reply
ISP doesn't help because this is my fail - bad soldering, short rts to the ground
0 项奖励
回复

1,185 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Sep 18 01:48:39 MST 2011
Did you try to switch to ISP already?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 项奖励
回复