Code Red, support for lpc24xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Red, support for lpc24xx

1,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Wed Apr 21 09:12:21 MST 2010
Hi,

Are there any plans for supporting OEM boards from Embedded Artists (LPC24x8, LPC32xx) (templates, examples, BSP's)? in the Code Red suite ?

BR
Morten Opprud

Original Attachment has been moved to: 1100321_dfuApp3578347110197385125.txt.zip

0 件の賞賛
返信
3 返答(返信)

1,064件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri May 14 05:37:03 MST 2010
No, support for lpc24xx will not be added to LPCXpresso
0 件の賞賛
返信

1,064件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by opprud on Fri May 14 04:21:07 MST 2010
Ok, i have looked at the comparison table and found the supported devices.

We plan to use the EA LPC2478OEM board and the LPC link for debug, for teaching sudents microprocessors, at Aarhus University in Denmark.
Are there any plans to add support for LPC24xx debugging, in the LPCXpresso tools.

BR Morten
0 件の賞賛
返信

1,064件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Apr 21 09:19:49 MST 2010
Hi,

The Red Suite products already support LPC24xx products and we hope to have LPC32xx support soon.

We don't support the EA boards directly, but they do provide a set of examples that can be used with Red Suite.

Hope that helps,
0 件の賞賛
返信